ATADAPCAN01, STK501 CAN Extension Kit support for the AVR AT90CAN128
Справочный проект от: Microchip Technology
ATADAPCAN01, STK501 CAN add-on is an extension to the STK500 and STK501 development boards from Atmel Corporation, adding support for the AVR AT90CAN128 device in a single development environment. The AVR AT90CAN128 includes a built-in Controller Area Network controller with all the features required to implement the CAN serial communication protocol in accordance with the BOSCH GmbH CAN specification