bq76925EVM Evaluation Module, Analog Front End for 3- to 6-Series Lithium-Ion Cells
参考設計 著者: Texas Instruments
BQ76925EVM is an Evaluation Module for BQ76925, Analog Front End for 3 to 6 Series Lithium-Ion Cells. The user's guide for the bq76925EVM evaluation module can assist designers in their evaluation of the bq76925, Analog Front End for 3- to 6-Series Lithium-Ion Cells. This guide discusses setup and operation of the module and contains schematics, bill of materials, and printed-circuit board layout. Before designing a battery management system with the bq76925, designers are advised to read the bq76925 data sheet If a designer wants to communicate with this EVM from a Windows-based PC, a separate USB Interface Adapter EVM is recommended. The USB-TO-GPIO Adapter serves as an interface adapter or a bridge between a host PC (IBM compatible) and one or multiple slave devices via a standard type-A to mini-B USB cable. The USB-TO-GPIO Adapter is listed below in the related tools section