线圈电感
A coil inductance calculator is a tool used to calculate the inductance of a coil of wire. Inductance is a property of an electrical circuit that describes the amount of energy stored in the magnetic field created by the current flowing through the circuit.
A coil of wire is a common example of an inductor. When a current flows through the wire, a magnetic field is created around the wire. The strength of the magnetic field depends on the amount of current flowing through the wire and the geometry of the coil.
The inductance of a coil of wire depends on several factors, including the number of turns in the coil, the radius of the coil, the length of the coil, and the spacing between the turns. A coil inductance calculator takes these factors into account and provides an estimate of the inductance of the coil.
To use a coil inductance calculator, you typically input the number of turns in the coil, the radius of the coil, the length of the coil, and the spacing between the turns. The calculator then uses a formula to calculate the inductance of the coil based on these parameters.
One commonly used formula for calculating the inductance of a coil is:
L = (μ₀ × n² × A) / l
where L is the inductance in henries, μ₀ is the permeability of free space (4π × 10⁻⁷ H/m), n is the number of turns in the coil, A is the cross-sectional area of the coil in square meters, and l is the length of the coil in meters.
Another commonly used formula for calculating the inductance of a coil is:
L = (μ₀ × n² × r² × π) / l
where L is the inductance in henries, μ₀ is the permeability of free space (4π × 10⁻⁷ H/m), n is the number of turns in the coil, r is the radius of the coil in meters, and l is the length of the coil in meters.
Using a coil inductance calculator can be helpful in designing electrical circuits that require inductors. By knowing the inductance of a coil, you can select the appropriate components and ensure that your circuit will operate as intended.
免责声明:
我们相信这些计算是准确的,但并不保证。使用时请自行承担风险!
Inputs
Number of Turns | N | ||
Loop Diameter | D | ||
Wire Diameter | d | ||
Relative Permeability | μR |
Output