Circuit shows a 2.5V output circuit using the LT1616
Thiết kế tham khảo bởi: Analog Devices
Circuit shows a 2.5V output circuit using the LT1616. The input range is limited on the low end by LT1616s under voltage lockout (3.6V max) and on the high end by the voltage rating of the capacitors used and the maximum voltage rating of the LT1616s BOOST pin