A000069, Arduino Mega2560 Development Kit Platform based on the ATmega2560 MCU, features an ATmega8U2 programmed as a USB-to-Serial Converter
Справочный проект от: Arduino S.r.l.
A000069, Arduino Mega2560 Development Kit Platform based on the ATmega2560. It has a USB host interface to connect with android based phones, based on the MAX3421e IC. It has 54 digital input/output pins (of which 15 can be used as PWM outputs), 16 analog inputs, 4 UARTs (hardware serial ports), a 16 MHz crystal oscillator, a USB connection, a power jack, an ICSP header, and a reset button. The MEGA ADK is based on the Mega 2560. Similar to the Mega 2560 and Uno, it features an ATmega8U2 programmed as a USB-to-serial converter