직사각형 순환 인덕턴스
A rectangle loop inductance calculator is a tool used to calculate the inductance of a rectangular loop of wire. Inductance is a property of an electrical circuit that describes the amount of energy stored in the magnetic field created by the current flowing through the circuit.
A rectangular loop of wire is a common example of an inductor. When a current flows through the wire, a magnetic field is created around the wire. The strength of the magnetic field depends on the amount of current flowing through the wire and the geometry of the wire.
The inductance of a rectangular loop of wire depends on several factors, including the length and width of the wire, the thickness of the wire, and the number of turns in the loop. A rectangle loop inductance calculator takes these factors into account and provides an estimate of the inductance of the loop.
To use a rectangle loop inductance calculator, you typically input the length and width of the wire, the thickness of the wire, and the number of turns in the loop. The calculator then uses a formula to calculate the inductance of the loop based on these parameters.
One commonly used formula for calculating the inductance of a rectangular loop is:
L = μ₀ × n² × a / (2 × b) × ln(2b / a)
where L is the inductance in henries, μ₀ is the permeability of free space (4π × 10⁻⁷ H/m), n is the number of turns in the loop, a is the width of the wire, and b is the length of the wire.
Using a rectangle loop inductance calculator can be helpful in designing electrical circuits that require inductors. By knowing the inductance of a rectangular loop, you can select the appropriate components and ensure that your circuit will operate as intended.
면책 조항:
이러한 계산이 정확하다고 믿지만 보장되지는 않습니다. 사용은 본인의 책임 하에 진행하세요!
Inputs
Number of Turns | N | ||
Loop Width | W | ||
Loop Height | H | ||
Wire Diameter | d | ||
Relative Permeability | μR |
Output