PCB Trace Width Calculator
A trace width calculator is a tool used to calculate the width of a trace on a printed circuit board (PCB). A trace is a conductive path on a PCB that carries electrical signals between components.
The width of a trace on a PCB is an important parameter that affects the resistance and current-carrying capacity of the trace. A trace that is too narrow may overheat or fail to carry the required current, while a trace that is too wide may waste board space and increase manufacturing costs.
A trace width calculator takes into account several factors to calculate the optimal width for a given trace on a PCB. These factors include the maximum current that the trace will carry, the thickness of the copper layer on the PCB, the temperature rise allowed for the trace, and the desired voltage drop across the trace.
To use a trace width calculator, you typically input the maximum current that the trace will carry, the thickness of the copper layer on the PCB, the temperature rise allowed for the trace, and the desired voltage drop across the trace. The calculator then uses a formula to calculate the optimal width for the trace based on these parameters.
One commonly used formula for calculating the optimal trace width on a PCB is:
W = (I × L × K) / (ΔT × H)
where W is the width of the trace in millimeters, I is the maximum current that the trace will carry in amperes, L is the length of the trace in meters, K is a constant that depends on the material properties of the trace and the ambient temperature, ΔT is the temperature rise allowed for the trace in degrees Celsius, and H is the thickness of the copper layer on the PCB in millimeters.
Using a trace width calculator can help ensure that the traces on a PCB are designed to meet the required specifications and that the PCB can operate reliably. By optimizing the width of the traces, you can reduce the risk of failure, improve the performance of the circuit, and minimize manufacturing costs.
면책 조항:
이러한 계산이 정확하다고 믿지만 보장되지는 않습니다. 사용은 본인의 책임 하에 진행하세요!