4010-DKPB434-BS, Demo Board for the Si4010 ARIB STD T-93 test results when operating in the 315 MHz frequency band
参考設計 著者: Silicon Labs
4010-DKPB434-BS, Demo Board for the Si4010 ARIB STD T-93 test results when operating in the 315 MHz frequency band. The results demonstrate full compliance under the ARIB STD T-93. All tests are performed using a 4010-DKPB434-BS with a matching network modified for 315 MHz. The results can be duplicated by using the same configuration. Two kinds of test signals were used for testing: OOK mode with 4.8 kbps data rate and FSK mode with 100 kbps data rate and 50 kHz frequency deviation