Current in Termination Resistors in Case of Short Circuit to Vbat Using TLE6250G and TLE6251G High Speed CAN Transceiver
Progetto di riferimento di: Infineon Technologies AG
Current in Termination Resistors in Case of Short Circuit to VBATT Using TLE6250G and TLE6251G High Speed CAN Transceiver. It shows the path of the current, in the case the termination is splitted (2x60 or 120) Ohm. The transceiver will limit the current to the ICANL_SC value, if the battery voltage is higher than 12V