SPI Slave to PWM Generation Reference Design

참조 설계 작성자: Lattice Semiconductor

SPI Slave to PWM Generation Reference Design

SPI Slave to PWM Generation Reference Design. Pulse width modulation (PWM) uses a rectangular pulse wave whose pulse width is modulated resulting in the variation of the average value of the waveform. Every PWM signal is a continuous succession of high and low pulses. In mobile phones and other consumer electronic products, the Light Emitting Diode (LED) is increasingly being used as a display backlight. PWM offers an ideal solution for LED controllers as the dimming intensity of the LED can be controlled by changing duty cycle and frequency of the pulse. This design provides a bridge between a Microprocessor and a PWM generator. The SPI slave interface is used to receive command data from an external SPI master. The command data in turn are used to set the frequency and duty cycle of the PWM. In this design the Embedded Function Block (EFB) in the MachXO2 device is used to generate the PWM signal

쿠키를 사용합니다

쿠키를 사용하여 경험을 개인화하고 기능을 개선합니다. "모두 허용"을 클릭하면 모든 쿠키 사용에 동의하는 것입니다. 쿠키. 자세한 내용은 개인정보 처리방침을 참조하십시오.